Downlink Setup (Advanced LTE FDD)

LTE employs a new network architecture made up of multiple Evolved Packet Cores (EPCs) that communicate with each other and with evolved universal terrestrial radio access network base stations (eNBs). Each EPC contains a Mobile Management Entity (MME) and a System Architecture Evolution Gateway (SAE). The eNB stations communicate with the EPCs, with each other, and with user equipment (UE).

Click Downlink in the tree view to open the Downlink node. The Downlink node enables you to set parameters of the cell, reference signal, and synchronization signals.

The Downlink parameters are described in Cell Parameters (Advanced LTE FDD Downlink), Reference Signal (Advanced LTE FDD Downlink), Positioning Reference Signals (PRS) - (Advanced LTE FDD Downlink), Synchronization Signals (Advanced LTE FDD Downlink), and Power Relevant Parameters (Advanced LTE FDD Downlink).

Click the Predefined Config. button to access a Closeddialog box from which you can select a base channel configuration.

To set up a fixed reference channel (FRC), click the button to open the DL FRC Wizard.